Crocodile Clips - A Complete Buyers' Guide | RS

Crocodile Clips – A Complete Guide

What are the different types of crocodile clip? Discover their uses and the types available in our guide.

Crocodile Clips Banner

What are Crocodile Clips and What Do They Do?

Crocodile clips are spring-loaded attachments with serrated edges and small teeth. They are typically made from steel or copper and are also known as alligator clips, plier clips, and battery clamps.

Crocodile clips are principally used to create flexible, temporary or experimental electrical connections in industrial settings or laboratories. For example, this could be between two wires or between an electrical lead and the anode or cathode of a device (i.e. the entrance and exit points of an electrical current).

In addition, crocodile clips are also frequently used in education to demonstrate the function of batteries, bulbs or circuitry. Meanwhile, larger crocodile clips are often used in garages and car maintenance, where they are used with battery chargers and jump leads or for welding operations, where they can also usefully absorb excess heat.

Crocodile clips also have some non-electrical functions – for example, attaching identification badges or entry passes to clothing, assembling models before glue or solder is applied, and for holding dentistry bibs in place. They also have a multitude of additional uses, including everything from suspending models to attaching tent ropes.

How to Use Crocodile Clips

If you are using a crocodile clip purely as a clamp to hold two objects in place, operation is normally straightforward. However, using clips to create an electrical connection is more complex. Follow the guidelines below to connect wires to a battery or similar electrical device using crocodile clips, then test the connection:

  • Firstly, ensure that all electrical items are disconnected from power

  • Use wire strippers to remove the plastic insulation from the end of the wire. A light pinch should be sufficient to cut through the coating, allowing it to be easily peeled away

  • Thread the now-exposed end of the wire through the hole at the back of the clip and then loop it around the fastening screw if one is available, before tightening to hold it in place. If there is no screw, you may need to crimp the wire to hold it in place, using a suitable crimp tool. Alternatively, there may be metal wings that can be bent into place using pliers in order to secure the wire

  • Apply solder. Create a small patch of molten solder by placing the end of the heated soldering iron against a roll of the substance, then apply the molten solder to the crocodile clip and wire connection and allow this to cool. Make sure to proceed with caution as soldering creates high temperatures

  • There is now a solid connection between the clip and the wire. Open the jaws by pinching the back and attach this to the battery or electrical device

  • Apply a standard voltage indicator to test and ensure that the current is flowing correctly

Crocodile Clip Types

The table below outlines some of the different types of crocodile clips available and explains their typical uses.


Crocodile Clip Image

Crocodile Clip Type

Crocodile Clip Type Uses

Insulated Crocodile Clip

Insulated crocodile clip

Creating electrical connections - the insulation protects users

Plastic Crocodile Clips

Plastic crocodile clip

Creating electrical connections - the plastic shell provides robust insulation

Heavy-Duty Crocodile Clip

Heavy-duty crocodile clip

Tasks involving high currents or heavy industrial equipment such as power generators, battery chargers, or welding tools

Micro Crocodile Clip

Micro crocodile clip

Suitable for a variety of precise tasks, including clipping test meters, grounding electrical equipment, and battery connections

Crocodile Clip Brands

With so many different brands to choose from, finding the ideal product for your requirements is simple when you shop with RS Components. The following is a selection of leading crocodile clip brands:

Crocodile Clip Insulation Material

Different types of insulation material are used in the manufacture of crocodile clips. Some of the most common insulation materials include:


Crocodile Clip Insulation Material

Insulation Properties


Acetate

Acetate is a reliable, heavy-duty insulation material


Glass Fibre Reinforced Nylon

A versatile, safe, and highly compatible insulating material


Molded PVC

A rugged insulation option


Nylon

Robust and affordable


PE

Provides full insulation with good plug compatibility


Polyamide

An ideal choice when a rigid connection is required


PP

Polypropylene is a high-strength insulation option


PS

Polystyrene is a widely used and adaptable insulating material


PVC

Polyvinyl chloride is a widely used and highly versatile insulating material


Rubber

Traditional rubber is a durable and reliable insulating material


Silicone

Silicone is flexible, compatible, and resistant to high temperatures


Tenite Acetate

This is a tough, resistant insulation option, making it ideal for use in handles


TPE

Thermoplastic elastomer is a versatile, widely-used material providing good insulation

FAQs

What are Crocodile Clips Made from?

Crocodile clips can be made from different materials but the most common include copper and steel. Different varieties of steel each offer varying benefits, as outlined below:

  • Stainless Steel is tough and resistant to corrosion, but it can be difficult to solder

  • Nickel-Plated Steel also offers good resistance to corrosion and is widely used in industrial crocodile clips

  • Gold-Plated Steel is ideal for clips which need to be highly conductive to electricity but is also more prone to wear than alternative types of steel

Meanwhile, copper is also widely used for clips which need to have a low level of electrical resistance. Crocodile clips used by mechanics for vehicle maintenance and repair are typically made from insulated copper.

What is the Difference Between Crocodile Clips and Alligator Clips?

There is no real difference between crocodile clips and alligator clips. As a general rule, the term ‘crocodile clip’ is widely used in the UK whereas ‘alligator clip’ is more widespread in the USA, but the two terms are usually used interchangeably.