웹사이트 개선 중입니다.
시스템 업그레이드로 로그아웃될 수 있습니다. 다시 로그인해 주세요.
시스템 업그레이드로 로그아웃될 수 있습니다. 다시 로그인해 주세요.
A Sounder Beacon is an alarm which has both audio and visual properties and is usually used in emergency situations, such as fire alarms for evacuations or on emergency vehicles to alert road users.The Sounder emits a loud audible alarm to raise an alert to a hazard, while the Beacon provides a clear visual alert - usually by a flashing indicator light through a coloured lens.Conventional Sounder Beacons are often used in commercial and industrial sectors and can be found in public places such as schools, warehouses, offices, construction sites, laboratories and industrial parks.These beacons are often used in emergency situations, such as fires, earthquakes, or other natural disasters, as a means of letting people know to evacuate an area before disaster strikes and take other precautions. Non-emergency situations can also be handled with them, e.g. to control traffic outside or at factories and construction sites, to alert workers of any hazards that may be present there.
Sounder beacons can be triggered manually, such as by pressing a button, or they can be set to activate automatically in response to certain conditions, such as the activation of a fire alarm or the detection of a gas leak. They may be powered by electricity or by batteries, depending on the specific needs of the application.The audio and visual alarms in Sounder Beacons are integrated, making it an enhanced warning device. They can come with different tones incorporating high frequencies, low frequencies and industry-standard frequency patterns. They have different coloured lenses to give an improved warning signal. There is a wide range of alarm system equipment options available for both indoor and outdoor use. Some Sounder Beacons are equipped with volume control and tunable features. Beacons may be constructed with halogen bulbs similar to those used in xenon flashtubes or LED floodlights.There are several types of sounder beacons, including flashing beacons, which use flashing lights to grab attention, and rotating beacons, which use a spinning light to create a strobe effect. Some sounder beacons also include a speaker or other audio component, which can be used to broadcast an alarm or other warning message.
Typically, the audio range of a sounder beacon will be between 5 and 15 decibels (dB (A)) above the ambient noise level. There are many considerations when working out the coverage of a sounder beacon, for example, you'll need to take into account any noise like the sound of people or machinery.It is important to note that sounder beacons should be used in conjunction with other safety measures and should not be relied upon as the sole means of alerting people to potential danger. In addition, it is important to follow any evacuation or other safety procedures that may be in place in the event of an emergency.
At RS we have a broad range of robust Sounder Beacons to fully suit your needs. We stock combined sounder and beacon products including klaxon sounder beacon, eaton sounder beacon, alarm sounder beacon from reliable brands such as Fulleon Flashni, Klaxon, e2s, Werma, Patlite, Schneider Electric and Moflash. We also have our own versatile RS range, specially designed and rigorously tested to high industry standards for maximum longevity, efficiency, protection, and ease of installation. With our RS Pro audio-visual alarm system solutions, you can trust that you will get exceptional quality for a great value.