Partnering with Leading Suppliers to bring you the toughest products for the harshest environments.

Making the right product choices for harsh environments

Electronic devices and systems located in harsh environments will always struggle to perform as required if they are not built with the appropriate components. A comprehensive understanding of the challenges to be faced by a device is required for effective product sourcing and buying for harsh environments. There are many environmental dynamics to consider: these include the extremes of temperature, mechanical stresses such as pressure or vibration, prolonged exposure to chemicals such as fuel and gases, or radiation and strong electromagnetic forces, or simply water, especially with its corrosive high-salinity content in marine applications.

Product Selection

The range of electronic components designed for harsh conditions is wide and extends from radiation-hardened semiconductors to doubly pinned passives to conformal-coated connectors to electrically isolated power supplies among many others including switches, relays and fans. Fundamentally, and it is a message of paramount importance to buyers, there is usually a good reason why a particular part in the bill-of-materials has been selected by the designer. A simple example is the design engineer’s selection of a bronze IP67-rated connector – protected against dust ingress and immersion in water – and its replacement with a cheaper aluminium device that also happens to meet IP67, but will not meet the demands of a saltwater environment. Another example is a power supply designed for use in an industrial automation application such as in a chemical- or food-processing plant. The product needs to be water, ice, oil and dust resistant, as well as being vibration and shockproof, able to handle high temperatures and also meet the appropriate rating for potentially explosive atmospheres.


Materials are a key element in the selection of products and buyers need to be cautious when trying to make cost savings as different materials offer some very different properties. Major manufacturers make standard interconnection product ranges in a wide variety of materials suitable for very diverse markets, as well as offering a wide range of mating cycles for heavy-duty applications. In addition, more bespoke interconnection products for highly specific harsh environments are available from manufacturers. Consequently it is worth considering using a distributor with broad range of suppliers and expertise in harsh environments, like RS, especially when purchasing relatively small quantities of a part.

Overall, a thorough understanding of target conditions is important to make the right product choice; but even so, this will be a compromise between several competing requirements. For example, aluminium is a lightweight and electrically conductive metal that offers wide application use, but it is vulnerable to saltwater. Plastic is much less vulnerable and is also lightweight, but it is not electrically conductive and can be vulnerable to UV radiation. If very high tensile strength is required, then both of these materials would be a poor choice compared to stainless steel, but this would have a considerable impact on weight. In addition, materials can be vulnerable in environments that might appear safe at first glance; for example, highly acidic fluids and aggressive chemicals are present in the common domestic environment in the form of orange juice and cleaning fluids.

Helping with Complexity

Overall, the selection of products for harsh environments can be a complex process – looking at attributes, materials or ratings in isolation provides just part of the picture. RS understands this well from our long experience in delivering components to a diverse range of businesses, in conjunction with a broad product range that will meet the demands of virtually all applications including some of the most specialist markets. Distributors such as RS can deliver a helpful and holistic service in selecting the right product for specific environments.

RS Pro - Performance and Quality you can trust

Electrical, Automation & Cables

Test & Measurement

Non-sparking Tools

Non-Sparking tools are tools that generate low energy sparks, always below the ignition energy of the hazardous substances (gas or dust) present in the environment. Non-Sparking tools are therefore called so whenever the sparks caused are always below lower ignition limit, and thus safe to use in explosive environments. Additional anti-corruption/ non-magnetic properties make them ideal for various harsh environment applications.

These tools are manufactured from commonly used materials to deliver non-sparking abilities, including copper-beryllium alloy (Cu-Be) and aluminium-bronze alloy (Al-Br). In addition to being non-sparking, these materials have non-magnetic properties and are also highly corrosion resistant, making them ideal for marine work in particular.

Leading Suppliers